10/30/2023 12:28 PM | |
Joined: 9/23/2005 Last visit: 11/4/2024 Posts: 4779 Rating: (728) |
It depends what are you going to do with it. Overview of possibilities. A manual for the mentioned module. In general the module is not meant for quadrature encoders.
Say there's continuous product moving at say 8 m/sec. And it is cut into pieces, say of 100 mm length. And there's some quality check device with sufficient sampling speed. @ 1 ms cycle time there's 8 mm window where product is suspected to have bad quality. Whenever cut happens in that window both pieces, before and after cut must be rejected. This yields 8% of excessive rejection. If oversampling x16 is used, this window shrinks to 0.5 mm. In turn excessive rejection drops to 0.5 %. |
Regards, |
|
This contribution was helpful to2 thankful Users |
Follow us on