1/12/2023 9:35 AM | |
Joined: 1/5/2022 Last visit: 9/5/2024 Posts: 18 Rating: (3) |
Hi In the past I have programmed CAN transparent communication using proxy. It was very tedious and prone to errors. In my current project however I am using this library. The documentation describes both configured messages and proxies but it seems like I only need the proxy. Q1: Q2: Q3: |
Last edited by: Jen_Moderator at: 01/12/2023 13:02:46Link optimized. |
|
11/4/2023 5:48 PM | |
Joined: 4/28/2015 Last visit: 2/7/2024 Posts: 10533 Rating: (820) |
Hello,
I've found this your old Topic but have answer to you and maybe for late searches. It looks to me from your screenshot that with this your exact settings all 11 bit ID messages can be received to buffer although Bit mask sets probably 29 bit ID allowed. In this case also that Bit verification of ID is all 0 it is also probbaly clear to have all messages with 11 bit criteria only to be received. In my opinion, if you'll set to Bit verification of ID some value f.ex. 0000000A then only message ID A will be proceeded to buffer. Update: I recommend also change name of Topic to see clearly that CM module of ET200SP HW is used here. There are also other CM modules with similar CAN functionality (on S7-1200 and also on ET200S HWs) so it can be then clear for users. |
Last edited by: Duris_I at: 11/05/2023 08:47:22With best regards... |
|
Follow us on