11/14/2023 9:14 AM | |
Joined: 7/26/2017 Last visit: 11/30/2023 Posts: 3 Rating:
|
This video illustrating how can I read but no how can I write value. I can read value but I cant write value |
11/15/2023 5:45 PM | |
Joined: 11/8/2017 Last visit: 8/13/2024 Posts: 328 Rating:
|
Hi, The recommended workflow for BACnet referencing has changed since the time that the video mentioned above was posted. The changes came with the release of V5.0. Refer to the attached screen dumps, where a summary of the workflow is shown. All of this is done from the main ABT window > Engineering > BACnet References. You will either need to use 'Read and Write' or 'Read and Command' when creating the output. 'Read and Write' is generally used for 3rd party points that have no priority array. 'Read and Command' is used for points that have a priority array. The type of point is shown in the 'Function' column within the Overview section. Note that it's also possible to import an EDE file created from a BACnet browser program. Once you have created your points, these can then be dragged and dropped into your software within the programming (TIA) tool. Regards, AttachmentCapture.zip (273 Downloads) |
Last edited by: CJ. at: 11/15/2023 17:46:51 |
|
Follow us on