11/29/2023 10:24 PM | |
Joined: 12/20/2020 Last visit: 4/27/2024 Posts: 15 Rating:
|
Hi All Any one can help with this problem; I am trying the commissioning a new CNC system 828d sw24x+ BLM+ DMM +SMM. Two motors with Cliq are connected to the DMM . However , both encoders are not identified and hence not shown in actual topology. EP is hooked to 24vdc for all drives. topology ,axes diagnosis and connections are shown in the attachment. When the system is switched on, the infeed is working and its fan is on I can hear that. However, the two drives no fan sound. All drives got green led. N main supply is connected to system yet, only 24vdc. therefore , the infeed works for few seconds and the switches off automatically. Any help to get the encoders detected? Thank you all. Attachmentenc prob.zip (234 Downloads) |
11/30/2023 8:13 AM | |
Joined: 12/20/2020 Last visit: 4/27/2024 Posts: 15 Rating:
|
here are more pics Only inputs X122.1 (OFF1) and X122.2 (OFF3) are connected AttachmentEncoder 2.zip (275 Downloads) |
Follow us on