(0)| 12/7/2023 7:41 AM | |
|
Joined: 1/19/2016 Last visit: 2/19/2025 Posts: 5 Rating:
|
Hi. I have the same issue with the drop down list in the recipe view as "Ufuk1985" describes. Its on a tp2200 comfort panel running on TIA V13. If I run the project in simulation on the computer the dropdown list shows almost all the data records (it fits the screen size), but when i download the exact same project to the HMI the list behaves as "Ufuk1985" describes and only shows a few data records, so a lot of scrolling needs to be done to select recipe. Any solution to this, some kind of runtime setting on the HMI etc? ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 12/07/2023 12:22:20New subject after splitting |
|
Follow us on