1/1/2024 8:44 PM | |
Joined: 4/21/2015 Last visit: 7/21/2024 Posts: 56 Rating:
|
Hi I want wiring diagram cable 6es7922-3bd00-0an0 Can anyone help me??? |
1/1/2024 9:27 PM | |
Joined: 9/27/2006 Last visit: 7/23/2024 Posts: 12270 Rating:
|
Hello;j mr j at; The unit you are looking for is refered to as a MTA (marshalling termination unit) for ET 200M stations in a PCS 7project. They are designed to simplify cabling and wiring between the ET 200M I/O modules and the I/O cabinet. They include an interconnecting cable, of course, such as the one for whuch you are showing the part number, but also a 20- or 40-pin front connector that attaches to the I/O module and and a connection board where you will bring the field wiring you want to connect. Look at the manual link provided by jkml in this thread for the information on the MTA modules : https://support.industry.siemens.com/forum/ca/en/posts/6es7922-3bd00-0at0-pin-assignment/27732 Note also that for the pin assignment information relative to the specific part number he was looking for, the O.P. in that thread had to contact Siemens directly, probably thrugh a Support Request: use the Support link at the top right of this page, select Create a Support Request and fill in the dialog boxes provided there. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 01/01/2024 21:39:01 |
|
Follow us on