1/24/2024 5:26 AM | |
Joined: 9/21/2012 Last visit: 11/4/2024 Posts: 4190 Rating: (470) |
Don't post the same question to multiple places. |
This contribution was helpful to1 thankful Users |
1/24/2024 10:34 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
Closed cause question posted twice. The second thread with the subject Controlling SEW MDX61B drive with S7 400 PLC via Profibus using DFP21B Gateway is published within the conference Decentral Peripherie. Jen_Moderator |
Follow us on