1/24/2024 9:06 AM | |
Joined: 11/22/2008 Last visit: 7/10/2024 Posts: 40 Rating:
|
Gears I'm making rTurning machine etrofit with Sinumerik One PPU1740. with PLC 6.15 basic software I have made ncessary change for turret managment and create INI file as attached. via by under Toolmanagement area. MD52200 =1 MD18080 = Bit 0,1,3 = 1 MD20310= Bit ,0,1,3 =1 Under the tool list i can see 12 position for turret . Issue is when i load the new tool ,tool loaded to loading location (not loading station) and when i checked the DB71 there is no active interface and no loading signal neither no loading station signal . So there is no comminication between PLC and NC at tool management side.. Can anyone advise how to activate interface between NC and PLC Thanks for support AttachmentTurret12_2.txt (119 Downloads) |
1/24/2024 11:54 AM | |
Joined: 11/22/2008 Last visit: 7/10/2024 Posts: 40 Rating:
|
Dear Mr Riddersholm Thanks for the support ! I m using Tia Portal V17 software and i can not find FB15 in Library. Here is the back up of my setup file. Best Regards Attachmentarchive (2).zip (144 Downloads) |
Follow us on