2/14/2024 10:40 PM | |
Joined: 8/17/2021 Last visit: 8/11/2024 Posts: 191 Rating: (3) |
Hi, What’s the process to update Desigo CC v4 to Desigo CC v6? Thanks |
2/15/2024 5:07 AM | |
Joined: 4/28/2015 Last visit: 8/12/2024 Posts: 84 Rating: (42) |
Hello, V4.0 --> V4.2 --> V6 Engineering Step-by-Step / Installing the Software / Upgrade Roadmap In Version 6.0, upgrade is supported only for Desigo CC Version 4.2 and above. No interim upgrades are supported. For example, upgrade from lower build number to higher build number of Desigo CC Version 6.0 is not supported. https://sid.siemens.com/r/A6V13910665/20851008651_22333429899__en-US_15175607307 Regards, Roger |
Last edited by: The Helping Hand at: 02/15/2024 10:56:20Text formatting optimized |
|
2/19/2024 5:39 AM | |
Joined: 4/28/2015 Last visit: 8/12/2024 Posts: 84 Rating: (42) |
Since I assume that you have an SI BP Partner account, I recommend that you bookmark SID. This is where you can find the latest documents and also the online help for V6 and V7. Upgrade Roadmap (V7 Engineering Help) The upgrade roadmap provides you with high-level tasks that are required to upgrade the Management Station along with all the installed prerequisites, language packs and extensions with the post-installation steps, if any. In Version 7.0, upgrade is supported only for Desigo CC Version 5.0 and above. No interim upgrades are supported. For example, upgrade from lower build number to higher build number of Desigo CC Version 7.0 is not supported. https://sid.siemens.com/r/A6V14198387/22837779723_22838076171__en-US_15175607307 Update Desigo CC application Just used to add extension modules and/or language packs of the same Desigo CC version. It is therefore not the same as the Update button you know from other applications that allows you to update the application to the latest version. |
Follow us on