2/25/2024 7:56 AM | |
Joined: 11/19/2021 Last visit: 5/16/2024 Posts: 29 Rating:
|
I am getting values from Modbus, and occasionally get spurious values. I can filter out most of them, but sometimes get a value of -10000 which is out of range of Logo (-32786 to +32768) so my filtering does not work. How can I filter this out? I attach the relevant section of the program.
AttachmentLOGO filtering.pdf (237 Downloads) |
2/25/2024 10:56 AM | |
Joined: 6/11/2019 Last visit: 8/30/2024 Posts: 2227 Rating:
|
Hello sjt01, If there is no error in the connection of the data that ixo65 suspects, you can program a workaround (see appendix). However, the final values of the logo area are already considered errors. It is better to connect the data to the logo correctly. Greetings Ella_68 (translated with Google) AttachmentProgrammplan-7.zip (244 Downloads) |
This contribution was helpful to
1 thankful Users |
Follow us on