3/15/2024 7:30 PM | |
Joined: 11/8/2017 Last visit: 7/12/2024 Posts: 328 Rating:
|
Hi, Yes, you can migrate a Desigo Insight project into Desigo CC. You need to use Desigo Insight V6 SP2 or higher to create the migration export (via Project Utility). You can either do this on your customer's management station (if they are running Desigo Insight V6), or you can do this on an engineering PC provided that you have an engineering dongle and license. Migration of graphics can be done, there is an Extension Module on Desigo CC that will allow you to do this. There is re-work required though on migrated graphics in order for the appearance to be acceptable, so please bear this in mind. You can also skip this part, and create new graphics based on the symbols libraries that are part of Desigo CC. See attached PDF for a basic summary of the migration process. Regards, AttachmentInsight to CC Migration Sales Guide.pdf (91 Downloads) |
Follow us on