3/11/2024 9:11 AM | |
Joined: 4/24/2006 Last visit: 7/31/2025 Posts: 9027 Rating:
|
Hello, Perhaps the following link might help: LOGO!-Library – Functions for analog value processing and communication Best regards, Wizard |
3/15/2024 10:09 AM | |
Joined: 12/27/2006 Last visit: 8/26/2025 Posts: 1200 Rating:
|
Calqulations is not nessesary. 1: Chose the right blok and make te next settinges a: Sensor 0 - 10V, or 0 - 20 mA or 4 - 20 mA b:Measurement range: min: -> 0 c: Measurement range: max => 3600 Ready! Look in the attachment AttachmentTreshiolt-Trigger.zip (514 Downloads) |
Follow us on