4/10/2024 12:11 PM | |
Joined: 4/27/2022 Last visit: 7/26/2024 Posts: 3 Rating:
|
Hello guys, I'm trying to connect Unified Comfort panel (MTP1500) to database. With MS SQL I have no issue but I'm trying to connect to PostgreSQL. With connection string should be possible only it looks like, Postgre driver is not installed on MTP (it is not written anywhere and I don't know how can I check it). Is there any way how to check if the Postgre driver is installed (need to define connection string correctly) or how to install it inside MTP panel? I have already checked this topic WinCC Unified: Use of SQLite or Microsoft SQL databases on FAQ. MS SQL connection string:
In text is written: Driver = Name of the driver used. The driver must be installed on the client.You can check the installed drivers in the "ODBC Data Source Administrator (64-bit)" ("Drivers" tab). |
Last edited by: Jen_Moderator at: 04/11/2024 06:04:21Link optimized. |
|
4/10/2024 8:37 PM | |
Joined: 1/21/2013 Last visit: 8/15/2024 Posts: 3044 Rating:
|
Hi Taurid_TL, WinCC Unified Comfort Panels currently support Microsoft SQL and SQLite. You cannot install your own ODBC driver on the panel. Kind regards |
Follow us on