8/23/2023 8:03 AM | |
Joined: 7/15/2022 Last visit: 8/2/2024 Posts: 7 Rating: (0) |
I have a problem with the web navigator menu and the toolbar it used to work but now it doesn't in the navigator, menu and the tolbar does not show in the navigator ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 08/23/2023 08:30:40New subject after splitting |
|
8/24/2023 9:28 AM | |
Joined: 8/3/2009 Last visit: 8/2/2024 Posts: 13446 Rating: (1703) |
Hello Sarvarjon Which Version of WinCC or WinCC Professional do you use exactly? can you send a screenshot? Do you use a webbrowser or the WinCCViewerRT? If you use a Webbrowser, then use the MainControl.html then you should see the webnav menue as a colored line to slide in If you use BPC then have also a look at this FAQ: https://support.industry.siemens.com/cs/de/en/view/109792636 Bye Murof |
Last edited by: Murof at: 08/24/2023 09:30:35If this Information really helps, you could use the Rate function |
|
4/21/2024 1:31 PM | |
Joined: 7/15/2022 Last visit: 8/2/2024 Posts: 7 Rating: (0) |
Hello i use wincc v7.4 and web navigator (web browser). |
Follow us on