4/19/2024 2:03 AM | |
Joined: 11/21/2023 Last visit: 4/19/2024 Posts: 2 Rating: (0) |
Hi, We recently had multiple sites with IoT2050s fail to reboot after a remote reboot command was issued. I've attached the log from one of the sites noting the failed reboot occurred on 16 April, from the log does anyone have any idea why the IoT2050 failed to reboot. On the 18 April a power cycle was able to successfully boot the device. Cheers David Attachmentfailed_reboot.txt (80 Downloads) |
4/21/2024 2:26 PM | |
Joined: 4/28/2015 Last visit: 6/28/2024 Posts: 578 Rating: (43) |
Might be https://github.com/siemens/meta-iot2050/issues/440 as well. That is only fully visible via the UART debug interface. |
5/16/2024 3:28 PM | |
Joined: 6/29/2018 Last visit: 6/21/2024 Posts: 3 Rating: (0) |
We face the same issue.. I have seen a hardware watchdog is available in iot2050 as posted here. Did someone use that feature to solve the problem of reboot ? Best Regards. |
Follow us on