5/21/2024 6:36 AM | |
Joined: 5/8/2024 Last visit: 5/30/2024 Posts: 8 Rating:
|
"The only thing that needs to be handled on the drives from the other CU is that you need to connect the enabled signal from the Smart Line Module to those drives. It is parameter p864 on the drives. By that parameter the axes "know" whether the Smart Line Module is enabled or not, which is important for enabling the drives. You could handover this enable signal via Digital I/Os from one CU to the other or via telegram if you communicate to your devices via PLC." Hey , can you pls explain this in details ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/21/2024 12:44:24New subject after splitting |
|
Follow us on