3/22/2021 10:52 AM | |
Joined: 3/11/2019 Last visit: 8/2/2024 Posts: 1540 Rating: (277) |
Dear PedroMendez, following FAQ can be helpful for this event. What should you do if the F-CPU goes into STOP mode and the message "Data corruption in the safety program ..." appears in the diagnostics buffer?regards sancruz |
Feedback appreciated, please rate |
|
This contribution was helpful to2 thankful Users |
4/24/2021 5:34 PM | |
Joined: 2/26/2020 Last visit: 12/18/2023 Posts: 6 Rating: (0) |
Hi @mopS04, and sancruz, I am facing this issue with an output in the F-program. I am already read the What should you do if the F-CPU goes into STOP mode and the message "Data corruption in the safety program ..." appears in the diagnostics buffer?In the buffer diagnostic, I get the alarm message of the error in the Q24 offset 1, as I read in the link provided, which means that the error is in Q24.1. My big problem is that this specific output is just written in one place as shown in the image attached. I am really struggling with this issue and I have no luck finding a solution can you advise me on something else, please. The information that maybe you should know is that the output is written just there and also the bit "emergenciesOK" is a static memory only to know if every emergency in the system is Ok. The code is very simple, so the error is weird in my point of view and I don't have any idea how to solve it. Please can you help me? |
4/24/2021 11:15 PM | |
Joined: 9/1/2017 Last visit: 7/9/2024 Posts: 156 Rating: (19) |
Hi
I think it means that the data corruption is in output byte 25 (second byte) of the F-DQ not Q24.1. Hope this helps Regards Hosein |
Last edited by: hosein8419 at: 04/24/2021 23:23:41 |
|
This contribution was helpful to2 thankful Users |
5/24/2024 2:30 PM | |
Joined: 9/27/2017 Last visit: 6/18/2024 Posts: 13 Rating: (0) |
Hello everyone. I am facing the same issue, did you find where the error were coming? Best regards. |
Follow us on