5/29/2024 8:23 AM | |
Joined: 5/29/2024 Last visit: 5/29/2024 Posts: 1 Rating: (0) |
I’ve installed my extended Farmbot Express (4.5 x 2.7m) and its working but the x axis running along the wood of the garden bed is often stalling, getting stuck and missing steps. I’ve got 2 spare NEMA 23 Closed Loop Steppers like this https://www.oyostepper.de/goods-587-Y-Serie-1-Achsen-CNC-Schrittmotor-Closed-Loop-Schrittmotor12-Nm-Nema-23-Motor-und-Schrittmotortreiber.html (except mine are 1.85Nm). Can I connect these stand alone stepper drivers to the Farmduino Express board? The huge extra torque and close loop system should resolve my issues. |
Follow us on