6/7/2024 10:20 AM | |
Joined: 12/29/2020 Last visit: 8/8/2024 Posts: 1 Rating: (0) |
I am trying to achieve the same functionality, as I made a custom keyboard for AlphaNumeric, NumericInteger & NumericReal Value. But What shall be the range of input is something the operator shall be aware. Does anyone have a solution to this? One that comes to my mind for now is to create internal HMI tags, mark them as Persistence Runtime, and link these tags to the lower2 and upper2 ranges. Also, display them on screen. But doing this is increasing the number of Tags also, work time. Please help me get another way to read Lower2 and Upper2 constant values using the script. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 06/10/2024 06:12:00New subject after splitting |
|
6/10/2024 7:12 AM | |
Joined: 1/21/2013 Last visit: 8/4/2024 Posts: 3044 Rating: (479)
|
Hi BaeRojgar, Since the WinCC Unified Object Model does not contain the tag limits, it would not be possible to get them using scripting. Kind regards |
Follow us on