6/10/2024 2:05 PM | |
Joined: 6/4/2024 Last visit: 6/12/2024 Posts: 1 Rating: (0) |
I am currently trying to update a device to the newest firmware version. Therefore I need to boot the device with the example image. After flashing the SD card with the example image v.1.1.1 the boot gets stuck at some point (see log). I already tried with multiple SD cards and flashing software. Also does not work if I try the same with booting from USB stick. Is there a different way of updating the firmware, so I could try then with the newer images/Industrial OS versions? Attachmentbootlog.txt (17 Downloads) |
Follow us on