8/3/2023 8:18 AM | |
Joined: 1/21/2013 Last visit: 8/4/2024 Posts: 3044 Rating: (479)
|
Hi EBRO_FP, What image version are you running on your MTP? As far as I know, this behavior was changed with V18 Update 1. So I would recommend downloading and installing the update. Kind regards |
8/3/2023 8:27 AM | |
Joined: 8/3/2009 Last visit: 8/8/2024 Posts: 13502 Rating: (1709) |
Hello EBRO_FP I think also in V18 Upd2 there are improvements regarding symbolic IO Fields. I had also an issue with symbolic IO Fields that was fixed with Upd2. Now it works... so perhaps you use the latest Upd (install also the latest Runtime Update, because this is also for simulation) Use and download also the Images V18.0.0.2 for Unified Comfort Panels: https://support.industry.siemens.com/cs/de/en/view/109746530 Bye Murof |
Last edited by: Murof at: 08/03/2023 08:28:59If this Information really helps, you could use the Rate function |
|
8/3/2023 8:35 AM | |
Joined: 7/27/2023 Last visit: 8/1/2024 Posts: 2 Rating: (0) |
Running version V18 update 1.
Okay thanks guys ill try updating to update 2. |
This contribution was helpful to1 thankful Users |
6/14/2024 12:15 PM | |
Joined: 10/30/2020 Last visit: 6/14/2024 Posts: 9 Rating: (0) |
Hello I am using MTP700 with firmware 18.0.0.3 but I still have this problem. See attached image. |
7/20/2024 7:11 PM | |
Joined: 1/8/2014 Last visit: 7/31/2024 Posts: 1 Rating: (0) |
Im facing the same issue in V19 update 2 |
Last edited by: Johan de Man at: 07/20/2024 19:13:11 |
|
7/22/2024 4:37 AM | |
Joined: 1/21/2013 Last visit: 8/4/2024 Posts: 3044 Rating: (479)
|
Hi all, This behavior will be fixed with V19 Update 3, according to my current knowledge. Kind regards |
Follow us on