2/21/2023 4:53 PM | |
Joined: 9/5/2022 Last visit: 7/24/2024 Posts: 2 Rating: (0) |
Hello, I have problem with my Thyristor controlled transformer, that uses Siemens SIPREC Sitouch panel v1.2. In the Pictures.zip file are 5 pictures where on the first one you can see what is only displayed on the touch panel. The menu button is greyed out and has no functionality. Anything tips would be useful. More details of the controller board are that is PIC 167-1, also pictures of the board are in the zip file. This thyristor controlled transformer is used to filter out gas to be more clean. Best regards, Jasmin AttachmentPictures.zip (539 Downloads) |
2/21/2023 5:12 PM | |
Joined: 2/21/2023 Last visit: 3/5/2023 Posts: 1 Rating: (1) |
Hello, I have the same problem and I can't solve it. If anyone has an idea, please let us know. |
3/23/2023 9:06 AM | |
Joined: 9/5/2022 Last visit: 7/24/2024 Posts: 2 Rating: (0) |
Did someone found any solution for this problem? |
Follow us on