6/25/2024 3:11 PM | |
Joined: 1/21/2013 Last visit: 7/12/2024 Posts: 2974 Rating: (469)
|
Hi MAMR_Deuser, Could you please tell us more about the system, especially the PLCs? What type of PLCs are you using? In general, WinCC Unified PC Runtime should be able to handle up to 128 connections to S7 PLCs and 50 connections to third-party PLCs when connected via Ethernet. Kind regards |
6/25/2024 3:13 PM | |
Joined: 2/10/2022 Last visit: 6/25/2024 Posts: 6 Rating: (0) |
4 PLC S7 1515F-2 PN |
Follow us on