6/19/2024 10:58 AM | |
Joined: 7/19/2022 Last visit: 6/28/2024 Posts: 373 Rating: (61) |
Hello AutoGen_7871185, On Unified panels you have to do it via Javascript. Here you have an application example: WinCC Unified PC Runtime: Control pop-up windows via script (JavaScript examples) |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to1 thankful Users |
6/26/2024 9:13 AM | |
Joined: 1/21/2013 Last visit: 7/12/2024 Posts: 2974 Rating: (469)
|
Hi M., OpenFaceplateInPopup is not available as a system function, but you can use it with JavaScript. Kind regards |
Follow us on