7/3/2024 6:06 AM | |
Joined: 5/22/2019 Last visit: 8/2/2024 Posts: 14 Rating: (3) |
Hello Isabela, I've taken a look into the manual of the PCS 7 Advanced Process Library. Anyways this sounds like a different problem for me (maybe even on the HW side), as it should be able to close the Valve with the Close command itself. Therefore I would recommend to find the cause of the problem instead of using a workaround (which is probably not possible without interfering with the internal logic). |
Last edited by: JK97 at: 07/03/2024 06:06:28 |
|
This contribution was helpful to1 thankful Users |
Follow us on