6/29/2024 10:04 AM | |
Joined: 10/3/2023 Last visit: 8/9/2024 Posts: 34 Rating:
|
Dear Experts, I have a Simodrive 611 (6SN1118-0NH11-0AA1). I got an error of E044 in my drive. So, I communicated my simodrive 611 with simoComU software through X471 port. As per manual, it said do a power on reset and then replace the option module. I done the power on reset through the SimoComU software. After the reset, My simodrive not communicating with the pc. It showing "Look for connected devices" and loading after that it showing try again or work offline. And, In drive display it is showing "-A" and after some values "1.1.1.6.d.3" like that it is showing. My question was how can i again communicate and connect with the software? I attached video for your reference. AttachmentNew folder (2).zip (37 Downloads) |
Follow us on