7/31/2021 12:26 AM | |
Joined: 7/8/2021 Last visit: 7/22/2024 Posts: 2 Rating: (0) |
Hello, I have a IPC677E with the software CPU1508(S7-1500), and I am using the port1 of the IPC for downloading the program and the port2 to communicate with the ET200SP. Initially I had several I/O modules on the ET200SP but all of them where unreachable. So I decided to keep it simple and just add a Server module. When I download the program and go online I have the error on the Server Module: A hardware component is or was inserted, but an error has occurred during module parameter assignment. * I made sure the name of the ET200SP is the same online and offline. * The firmware version of the Server Module or any other I/O is not displayed when I am going online. The firmware version of the Server Module matches. I am attaching several images of my configuration. Thank you so much, Luis AttachmentCaptures ET200SP.zip (361 Downloads) |
3/13/2024 6:20 PM | |
Joined: 12/11/2021 Last visit: 4/6/2024 Posts: 1 Rating: (0) |
I had the same problem. Thank you! |
7/12/2024 4:06 AM | |
Joined: 9/21/2012 Last visit: 7/22/2024 Posts: 4030 Rating: (454) |
Have a look on this document Attachment29430270_Config-Control-Modular_DOC_V31_en.pdf (4 Downloads) |
Last edited by: Wit_Moderator at: 07/12/2024 12:58:54File attached from link |
|
Follow us on