7/12/2024 1:52 PM | |
Joined: 7/10/2024 Last visit: 7/16/2024 Posts: 3 Rating:
|
Hello! Regardless of whether it is an ITP1000 or a PC, the way to configure the runtime advanced is the same. You will need to include a PC Station in the TIA Portal and insert both the WinCC RT Advanced component and the network card and make the HMI connection between the RT Advanced and the PLC. In this FAQ: https://support.industry.siemens.com/cs/af/en/view/89852595 you will find how to perform these steps. I hope it works |
7/17/2024 8:03 AM | |
Joined: 7/21/2023 Last visit: 7/17/2024 Posts: 10 Rating:
|
It's only example because i have ITP1000 and on screenshot is KTP900F but errors are the same. |
Follow us on