7/17/2024 9:31 AM | |
Joined: 3/14/2008 Last visit: 10/3/2024 Posts: 2105 Rating: (940)
|
Hi, The PC internal is sort of a virtual bus which can communicate with different protocols. For this to work, you need to work with the Station Configurator where the NetPro connection data is being download to. When the configuration is downloaded to all stations (connected to plant bus), you can communicate via PC internal. For your ES: 1. Save and compile NetPro for ES project 2. Select the PC station of the ES and right click->PLC->Configure. Now you can transfer the configuration to the ES, after configuration has been completed, select PLC->Download to download the configuration. |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
Follow us on