7/17/2024 10:47 AM | |
Joined: 5/30/2022 Last visit: 7/25/2024 Posts: 555 Rating: (94) |
Hi BELAL 399, It is not possible to restore a backup made by prosave between two different screens. You must first have the original OP 37 program. This screen, I seem to remember, is only programmed in protool so you would first have to do the migration to wincc flexible: SIMATIC HMI WinCC flexible 2008 WinCC flexible 2008 Migration and then from wincc flexible to TIA Portal: Or create from scratch the program already in the current screen.
|
If this information really helps, you could use the Rate function. |
|
7/18/2024 8:41 AM | |
Joined: 8/3/2009 Last visit: 7/26/2024 Posts: 13385 Rating: (1699)
|
Hello BELAL 399 I have not much experience in Protool but perhaps it works similar to Wincc Flexible https://support.industry.siemens.com/cs/de/en/view/98784532 Bye Murof |
Last edited by: Murof at: 07/18/2024 08:42:04If this Information really helps, you could use the Rate function |
|
Follow us on