7/20/2024 9:59 AM | |
Joined: 8/15/2010 Last visit: 10/4/2024 Posts: 9 Rating: (0) |
[snip...] When operating with the external handwheel, it was now noticed that in the Z axis position, depending on the fine setting 1-10-100, the axis also moves as desired. Charly ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 07/31/2024 11:04:43New subject after splitting Last edited by: Moderator_Lan at: 07/31/2024 11:06:53Last edited by: Moderator_Lan at: 07/31/2024 11:08:30Division of questions into seperate topics |
|
7/22/2024 12:09 PM | |
Joined: 5/24/2016 Last visit: 10/3/2024 Posts: 354 Rating: (52)
|
Hello. Good to hear that it worked out with the gear change. now in regards to you're other question. It is because the axis does in fact move the increment, but this would be on the linear axis. So this would equivalent in diameter to the double amount. You can adjust this in MD MD 31090 on the axis. Please look at this attached video for and example. Best Regards Riddersholm AttachmentChange Increment distance MD31090.zip (113 Downloads) |
Last edited by: Riddersholm at: 07/22/2024 12:09:43 |
|
Follow us on