7/23/2024 12:20 PM | |
Joined: 4/28/2009 Last visit: 7/24/2024 Posts: 347 Rating:
|
Hello, for control G120 drive from HMI you can use HMI direct access, application examples are here or here. Speed setpoint in telegram is specialy coded as integer. It is 16-bit (NSOLL_A, f.e. in telegram 1) or 32-bit PZD (NSOLL_B, f.e. in telegram 2). Principe of 16-bit coding is following: 4000h (16384) corresponding to 100% of reference speed in p2000 in drive. Range for positive speed is from 0 to 7FFFh (0..200% of ref.speed), for negative is from 8000h to FFFFh (-200..-1% of ref.speed). With regards |
Follow us on