7/24/2024 8:46 AM | |
Joined: 7/19/2022 Last visit: 10/18/2024 Posts: 403 Rating: (65) |
Hello AutoGen_6548995, On the part of the PLC, and following the instructions in the FAQ that it indicates, I would verify point 4.4 on page 20, specifically sections 3 and 4 where it is necessary to make a call in OB100 to reset the "Startup" variable and another in OB1 to reset the same variable. Are you doing this step? |
If this Information really helps, you could use the Rate function |
|
7/24/2024 2:09 PM | |
Joined: 6/10/2020 Last visit: 10/12/2024 Posts: 28 Rating: (0) |
hello, Thanks for your reply! I also did that please see the screenshots below. I created db1000 for section 1 in the FAQ, and inserted the logic to OB1 and OB100. It doesn't work also so I tried a dummy to manually enable the FB1000...The FAQ doesn't explain what M1.0 means. How do I define M1.0? Thanks again!
|
Last edited by: AutoGen_6548995 at: 07/24/2024 14:16:07 |
|
7/26/2024 8:36 PM | |
Joined: 6/10/2020 Last visit: 10/12/2024 Posts: 28 Rating: (0) |
hello, I have updated the logic of step3 and 4 and looks like the block got initialized, but always got fault. I'm using 410 plc x5 port to connect a cu320 unit so I select locdevid as 16#05, and use 99 (randomly selected one) for OUC connection id. Is there any other tricks to make it work? Thank you!
|
8/27/2024 10:33 AM | |
Joined: 6/27/2017 Last visit: 10/14/2024 Posts: 25 Rating: (0) |
Hi, How to identify the LocDevID? I'm using the port X8 of cpu 410E
|
Follow us on