7/29/2024 8:08 PM | |
Posts: 2 Rating:
|
I am using a VM to setup an ES/OS single station test project however I am not able to configure the PC Station. Please see my steps below and let me know if you have any suggestions of the issue.
I think I am doing something wrong when setting the IP address for the IE general but I do not know what IP address to use other than the one for the network adapter. As I said I am pinging the VM via the host name PCS7ES01 but when I go to configure the PC Station there are no accessible computers on any network. AttachmentTest Project - Pictures.pdf (302 Downloads) |
Follow us on