8/29/2024 7:00 PM | |
Joined: 7/2/2024 Last visit: 3/13/2025 Posts: 11 Rating:
|
Sorry, i thought is was clear "So in basic if input i1 is on, output Q1 is on and output Q2,Q3 and Q4 needs to be off. If input I2 is on, output Q1, Q3 and Q4 needs to be off. etc." In basic the logo program for the pump is what you send me, the rest is a separate programs and putting them al together in the end. (lights, valve's etc, all working) The Tia part is for now the tags and the press key function as showed in the pdf attachment. Very much thanks for all your help! AttachmentTia.pdf (495 Downloads) |
8/30/2024 2:28 AM | |
Joined: 12/18/2014 Last visit: 9/15/2025 Posts: 35962 Rating:
|
In attachment a litte project. TIA V16, LSC for a 0BA8.Standard. You have to change in TIA the IP addresses in the connection to your IP addresses. I have tested the project with a real LOGO! and HMI simulation. [Snip...] AttachmentAutoGen_1689549.zip (442 Downloads) |
Last edited by: Moderator_Lan at: 08/30/2024 06:56:10Link removed and added file as an attachment. |
|
8/31/2024 10:36 AM | |
Joined: 7/2/2024 Last visit: 3/13/2025 Posts: 11 Rating:
|
Thank you! The resetbit in Tia was what i did not think about.. good one :-) |
Follow us on