8/20/2024 8:02 PM | |
Joined: 7/19/2022 Last visit: 9/5/2024 Posts: 1 Rating: (0) |
Hi, Denilson. I'm testing the color palette feature and noticed that it's possible to access the DefaultColorPalette via HMIRuntime.UI.DefaultColorPalette. However, I'm unable to set or retrieve the currently configured object from the Runtime Settings. I created two objects in the Libraries, DarkTheme and LightTheme, with LightTheme as the default, which I set in the Runtime Settings. When I simulate the project, all the configured colors work perfectly. Now, I'm looking for a way to switch to DarkTheme by pressing a button or triggering another event. Any guidance would be greatly appreciated! ------------------------------------------------------------------------------------------ |
Last edited by: asvr at: 08/20/2024 20:26:52Last edited by: Moderator_Lan at: 08/21/2024 07:04:52New subject after splitting |
|
Follow us on