4/2/2024 9:21 AM | |
Joined: 10/25/2022 Last visit: 9/24/2024 Posts: 18 Rating: (6) |
Hi ixo65, Thank you for the library. The blocks seem to be password protected. I can not find the password in the documentation pdf in the link. I don't have any solar panels, i just wanted to see how the tracking is done ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 09/17/2024 07:09:46New subject after splitting |
|
4/2/2024 11:28 AM | |
Joined: 3/11/2019 Last visit: 9/6/2024 Posts: 1569 Rating: (289)
|
Hi,
That's the point. The blocks are protected via Know-How protection. I have never seen a library from Siemens which was Know-How protected and at the same time the password was published. This would not make any sense, otherwise Siemens would have released the blocks without any protection. So the conclusion is. It's not wanted to be able to see the code, only to use the blocks as they are described. You can have a look at the LGF library. There are blocks like "4.2.5 LGF_AstroClock (FB / V3.0.1)" to track sunrise sunset based on GPS coordinates. Maybe it is somehow used, or you can build something own with it. Library of general functions (LGF) for SIMATIC STEP 7 (TIA Portal) and SIMATIC S7-1200 / S7-1500regards sancruz |
Feedback appreciated, please rate |
|
This contribution was helpful to1 thankful Users |
9/11/2024 1:01 PM | |
Joined: 9/9/2024 Last visit: 9/16/2024 Posts: 2 Rating: (0) |
What is the password of the SPA Library????? |
9/14/2024 6:31 AM | |
Joined: 12/18/2014 Last visit: 9/26/2024 Posts: 33840 Rating: (4206) |
Read the documentation. |
This contribution was helpful to1 thankful Users |
Follow us on