10/2/2024 3:26 PM | |
Joined: 8/12/2024 Last visit: 5/14/2025 Posts: 2 Rating:
|
Hi, I try to read out the standard VM address of a logo 8 with an Ewon Flexy 205. No problem to read out digital in or outputs, using the S7access (protocol like reading I3 in logo using S73&400 with I0#2 by Ewon) But it seems the virtual VM mapping itself is not accessible. I can't read out Flag's (Merker) or analogue values. For example: IA3 in the Logo 8 is an analog input reading a level, following the VM mapping in Logo8, this should be readable at VM1036. Ewon allows modifiers: I, C, T, M... Tried to use MW1036 and many other addresses, modifiers, etc never a usefull result, but some random numbers, 0 -1 - 65284... there is communications, but where to find the correct mapping address, are those shifted ? It seems the VM mapping is accessible, but not with those adresses in de pdf Thanks for assistance! Greg AttachmentLOGO! 0BA8 Reserved VM addresses.pdf (331 Downloads) |
Follow us on