10/25/2024 1:34 PM | |
Joined: 2/7/2023 Last visit: 12/10/2024 Posts: 9 Rating:
|
Am I the only one getting constant "internal server error" issues when I access the forum? Anyway, I think I have figured it out. The code is NOT elegant, because I was adding all kinds of extra checks here and there... but it works. The only thing you have to do to make the code work is it needs the three demand inputs to be off at the same time, then it starts working properly, and from there it seems perfect. Attachmentround_robin_test_FUNCTIONAL.zip (294 Downloads) |
10/25/2024 1:36 PM | |
Joined: 2/7/2023 Last visit: 12/10/2024 Posts: 9 Rating:
|
These constant "internal server error" issues are killing me. This is my last attempt to upload. I think I have figured it out. Attachmentround_robin_test_FUNCTIONAL.zip (288 Downloads) |
This contribution was helpful to
1 thankful Users |
10/29/2024 10:10 AM | |
Joined: 2/7/2023 Last visit: 12/10/2024 Posts: 9 Rating:
|
I have been having a HECK of a time trying to access this forum. Constant internal server errors. Horrible. I installed Chrome to use instead of Firefox and that seems to have fixed the problem. I'm not sure what the deal was, there, but at least I can log in. I solved my problem, so I'm going to upload it here so that the next person doesn't have to reinvent the wheel. This version works, but it has two issues - you need to 'reset' it by having it start with no demand. If it starts up with all of the demand inputs turned on it will freak out. As long as it can reach a zero-demand state then it will get its bearings and it will be fine from there - even with demand on every input. The other issue is just that it has a lot of double-checking going on. It's not the leanest programming that I have done - that's for sure - but it works, and I haven't bothered going back to try to trim out what might not be needed. Anyway, the working version is attached. Attachmentround_robin_test_FUNCTIONAL.zip (284 Downloads) |
This contribution was helpful to
2 thankful Users |
Follow us on