8/4/2024 5:42 PM | |
Joined: 5/26/2011 Last visit: 9/16/2025 Posts: 483 Rating:
|
Hi experts, I really hope someone can help because our current problem is urgent We are upgrading PCS7 v8.2 CEMAT blocks to v9.1 CEMAT Minerals. Our issue is on Simocode, which uses C_SIMO_A block from ILS_CEM library. C_SIMOS is the one recommended since V7.0, but C_SIMO_A is the one working in V8.2 using C_SIMOS pdl graphics. The faceplate of the simocode appears as a pop up window from the "SIMOCODE" button on C_DRIVE faceplate. Now our problem is, in V9.1 CEMAT Minerals, this C_DRIVE faceplate has completely new appearance. The Simocode pop up button still exist ("SI" button) but it is greyed-out (cannot be clicked). I cannot fully understand the very different script on v9.1 on how he calls the Simocode pop-up faceplate from the newer C_DRIVE faceplate, I just copied the old C_SIMOS faceplate PDLs from V8.2 to our V9.1 project. Since we also use the same C_SIMO_A program block and do the similar naming convention xx_SC (though now v9 from ILS_CEM Lib), I expect that it should work as before. But maybe it now calls a different name for the C_SIMOS faceplate PDLs, or maybe there's new name syntax for the C_SIMO_A block that's why it cannot be clicked now? For information we are still simulating, Simocode not yet connected. Please see attached Simocode popup buttons events scripts. Any input will be highly appreciated! Thanks a lot. AttachmentSIMOCODE BUTTON EVENT.zip (319 Downloads) |
Last edited by: G_R_E_Y_31 at: 08/04/2024 17:53:28Last edited by: G_R_E_Y_31 at: 08/04/2024 17:56:02 |
|
Follow us on