7/1/2023 6:59 AM | |
Joined: 6/11/2021 Last visit: 8/31/2023 Posts: 13 Rating: (0) |
Dear Sir/Madam I'm Working with SICAM CP8050. In my connection, I use CP8050. as Modbus, IEC60870-5-104, IEC61850 master/client to connect to filed Deivce. At the assign step, I could assign the signal to Modbus and IEC61850 Station, but couldn't not do that with IEC60870-5-104, The error in below picture How can I fixx it? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 07/03/2023 08:38:38New subject after splitting |
|
This contribution was helpful to1 thankful Users |
12/16/2024 3:17 PM | |
Joined: 12/16/2024 Last visit: 12/24/2024 Posts: 1 Rating: (0) |
Getting the same issue here. Did you get answer for your question?
|
Follow us on