(0)| 12/9/2024 9:14 AM | |
|
Joined: 12/9/2024 Last visit: 12/9/2024 Posts: 1 Rating:
|
Assistance Required for Siemens G120 Drive Torque Limit Settings Dear Siemens Support Team, I am using a Siemens G120 drive with a 3 kW motor. The current limit is set to 7 amps, and the motor runs normally with a current draw of 3 to 4 amps under typical conditions. However, when a heavy load is applied, the motor current rises to 5 amps, and the torque goes to 12 amp, causing the drive to trip. I have already set parameterP1520to 45 but the issue persists. Could you please guide me on how to correctly adjust the torque limit settings to prevent tripping during heavy load conditions? Here are some additional details of my setup:
I would greatly appreciate any advice or recommended adjustments to resolve this issue. Thank you for your support! ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 12/09/2024 10:53:40New subject after splitting |
|
Follow us on