3/14/2025 3:39 PM | |
Joined: 11/15/2024 Last visit: 3/21/2025 Posts: 5 Rating:
|
Hello everyone, I am trying to do a back transfer from an MP177 multi panel, the option was indeed enabled when the project was first loaded by the manufacturer. we have the SAVEDATA.PDZ file in this location "\Storage Card MMC\Simatic\". The transfer parametre are configured on ethernet both on the panel and the PC with the correct IP adress. but i have an error message that says "Couldn't find the .PDZ file" . i followed all the steps given in siemens PDF file about back transfer the only thing that they say about this error is to check the location of the file and that the file must be named SAVEDATA.PDZ which in my case is accurate. I am using WINCC Flexible 2008 SP5 Updt 2. Please help me i would really appreciate it |
Last edited by: AZIWAL at: 03/14/2025 15:41:33 |
|
3/18/2025 1:54 PM | |
Joined: 4/24/2006 Last visit: 3/31/2025 Posts: 8920 Rating:
|
Hello, Please check directory on Panel. Go to Control panel -> Transfer settings Go to tab directories and check if the Backtransfer file go to the right directory (Project backup) Also be sure the directory is: correct and ends with backslash Can you check the Memory card on a PC? Best regards, Wizard |
We are working on a new user interface with better overview and more relevance.
Follow us on