(0)| 3/20/2025 7:01 AM | |
|
Joined: 8/13/2023 Last visit: 4/12/2025 Posts: 1 Rating:
|
hi i am facing an issue with the s7-300 plc, PLC going to Stop mode during running time. report as attached. kindly check and advice. both stop and run mode blinking. later i have to connect to laptop and do warm restart the PLC. Diagnostic buffer of module CPU 315T-2 DP Order No./ Description Component Version 6ES7 315-6TG10-0AB0 Hardware 3 - - - Firmware V 2.6.5 Boot Loader Firmware expansion A 10.13.9 Technology (312141) Firmware expansion V 3.1.1 Rack: 0 Slot: 2 Serial number: S C-W6V592402008 Event 1 of 10: Event ID 16# F360:B416 Fault in the encoder on the logical address E330 , fault message: 2h Incoming event 12:58:47.047 PM 04/15/1994 (Coding: 16# F360 B416 C050 014A 0000 0002) Event 2 of 10: Event ID 16# 4302 Mode transition from STARTUP to RUN Startup information: - Time for time stamp at the last backed up power on - Single processor operation Current/last startup type: - Warm restart triggered by switch setting; last power on backed up Permissibility of certain startup types: - Manual warm restart permitted - Automatic warm restart permitted Last valid operation or setting of automatic startup type at power on: - Warm restart triggered by switch setting; last power on backed up Previous operating mode: STARTUP (warm restart) Requested operating mode: RUN Incoming event 12:44:40.511 PM 04/15/1994 (Coding: 16# 4302 FF68 C700 0000 0813 7713) Event 3 of 10: Event ID 16# 1381 Request for manual warm restart STOP due to: Power failure Startup information: - Startup without modified system configuration - No difference between setpoint and actual configuration - Time for time stamp at the last backed up power on - Single processor operation Current/last startup type: - Warm restart triggered by switch setting; last power on backed up Permissibility of certain startup types: - Manual warm restart permitted - Automatic warm restart permitted Last valid operation or setting of automatic startup type at power on: - Warm restart triggered by switch setting; last power on backed up Requested OB: Startup OB (OB100) Priority class: 27 Incoming event 12:44:40.508 PM 04/15/1994 (Coding: 16# 1381 1B64 C772 494E 0813 7713) Event 4 of 10: Event ID 16# 4301 Mode transition from STOP to STARTUP STOP due to: Power failure Startup information: - Time for time stamp at the last backed up power on - Single processor operation Current/last startup type: - Warm restart triggered by switch setting; last power on backed up Permissibility of certain startup types: - Manual warm restart permitted - Automatic warm restart permitted Last valid operation or setting of the automatic startup type at power on: - Warm restart triggered by switch setting; last power on backed up Previous operating mode: STOP (internal) Requested operating mode: STARTUP (warm restart) Incoming event 12:44:39.885 PM 04/15/1994 (Coding: 16# 4301 FF46 C772 494E 0813 7713) Event 5 of 10: Event ID 16# 38C4 Distributed I/Os: station return Address of the affected DP slave: station number: 20 DP master system ID: 1 Log. base address of the DP slave: Input address: 2033 Log. base address of the DP master: 2047 Requested OB: Rack failure OB (OB86) OB not found, or disabled, or cannot be started in the current operating mode External error, Outgoing event 12:44:39.553 PM 04/15/1994 (Coding: 16# 38C4 FE56 C054 07FF 07F1 0114) Event 6 of 10: Event ID 16# 38C4 Distributed I/Os: station return Address of the affected DP slave: station number: 19 DP master system ID: 1 Log. base address of the DP slave: Input address: 2034 Log. base address of the DP master: 2047 Requested OB: Rack failure OB (OB86) OB not found, or disabled, or cannot be started in the current operating mode External error, Outgoing event 12:44:39.481 PM 04/15/1994 (Coding: 16# 38C4 FE56 C054 07FF 07F2 0113) Event 7 of 10: Event ID 16# F260:B119 Station recovery, DP(Drive) station: 7 Outgoing event 12:44:39.423 PM 04/15/1994 (Coding: 16# F260 B119 C050 0007 0000 0000) Event 8 of 10: Event ID 16# 38C4 Distributed I/Os: station return Address of the affected DP slave: station number: 17 DP master system ID: 1 Log. base address of the DP slave: Input address: 2037 Log. base address of the DP master: 2047 Requested OB: Rack failure OB (OB86) OB not found, or disabled, or cannot be started in the current operating mode External error, Outgoing event 12:44:39.409 PM 04/15/1994 (Coding: 16# 38C4 FE56 C054 07FF 07F5 0111) Event 9 of 10: Event ID 16# 38C4 Distributed I/Os: station return Address of the affected DP slave: station number: 16 DP master system ID: 1 Log. base address of the DP slave: Input address: 2038 Log. base address of the DP master: 2047 Requested OB: Rack failure OB (OB86) OB not found, or disabled, or cannot be started in the current operating mode External error, Outgoing event 12:44:39.337 PM 04/15/1994 (Coding: 16# 38C4 FE56 C054 07FF 07F6 0110) Event 10 of 10: Event ID 16# 38C4 Distributed I/Os: station return Address of the affected DP slave: station number: 15 DP master system ID: 1 Log. base address of the DP slave: Input address: 2039 Log. base address of the DP master: 2047 Requested OB: Rack failure OB (OB86) OB not found, or disabled, or cannot be started in the current operating mode External error, Outgoing event 12:44:39.265 PM 04/15/1994 (Coding: 16# 38C4 FE56 C054 07FF 07F7 010F) AttachmentDiagnose20032025.txt (248 Downloads) |
Follow us on