3/26/2025 11:40 PM | |
Joined: 12/14/2024 Last visit: 3/31/2025 Posts: 5 Rating:
|
I am controlling a Sinamics G120C-pn with a 1513 cpu. I am using the telegram 1 because I will handle the speed with a Technological Object (TO_Speed) and it only accepts specific telegrams. Since I need more info from the drive I extended the telegram by 2 words and I linked PZD3 to motor temperature and PZD4 to Phase current U V W. Is it how I am supposed to use the extended telegrams ? What are the PZD2&3 and PZD3&4 ? How could I use them and map them to my plc addresses? |
Last edited by: AutoGen_4189346 at: 03/26/2025 23:41:19 |
|
3/26/2025 11:40 PM | |
Joined: 12/14/2024 Last visit: 3/31/2025 Posts: 5 Rating:
|
|
3/30/2025 6:02 PM | |
Joined: 9/21/2012 Last visit: 4/1/2025 Posts: 4352 Rating:
|
PZD 1 & 2 are in use for Telegram 1 now. If you want to use the later ones, define Telegram extension in the HW config for the drive, and config as many words to it as you need. Then define the send/recieve data to the drive. |
We are working on a new user interface with better overview and more relevance.
Follow us on