4/2/2025 4:29 AM | |
Joined: 3/30/2020 Last visit: 9/15/2025 Posts: 5451 Rating:
|
You wish to fit a REAL number into a 16-bit variable. The S7-200 does not have a native data type that is a 16-bit floating number (https://en.wikipedia.org/wiki/Half-precision_floating-point_format). But it may be helpful if you could explain a bit more as to what you want to do. I will take some guessing. (a) DISPLAY
Keep in mind that the DINT variable has x2 16-bit words. VD200 is composed of VW200 and VW202. If the number is small enough: VD200 equals VW200. (b) COMMUNICATION |
Last edited by: qwazee at: 04/02/2025 18:47:07** VW memory words are found in the S7-200 PLCs Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
This contribution was helpful to
3 thankful Users |
Follow us on