(0)| 4/8/2025 6:21 PM | |
|
Joined: 5/6/2022 Last visit: 11/27/2025 Posts: 589 Rating:
|
Hi ToniVK, In this case, the first thing I think you should check is the following: - When trying to simulate a Unified Comfort Panel, the Unified PC Runtime has to be additionally installed on the device. If the Unified PC Runtime is missing on your system, you can find the downloadlink in following SIOS entry: "SIMATIC WinCC Unified PC Runtime V19 Simulation & Trial": https://support.industry.siemens.com/cs/ww/en/view/109820988 I understand that this is installed from what you indicate, right? - It would be helpful if you could attach a screenshot of the installed versions and the operating system you are working with. - Please attach a screenshot of the error. - Attach a screenshot of the Unified Runtime Manager to see the status of the project. - Does the same thing happen with any project you try to simulate or just with one in particular? Could you create a very simple panel project and try to simulate it? We look forward to your feedback! |
|
If this Information really helps, you could use the Rate function |
|
| 4/13/2025 6:08 AM | |
|
Joined: 3/16/2015 Last visit: 11/27/2025 Posts: 4 Rating:
|
Hi, Any advice still? I also tried to install everything again but without success. |
| 4/14/2025 1:17 PM | |
|
Joined: 8/3/2009 Last visit: 12/19/2025 Posts: 16612 Rating:
|
Hello ToniVK you could try to check if you have set up your certificates correctly: https://support.industry.siemens.com/cs/de/en/view/109806850 If this do not work You shuld create a Service Request at Siemens Support. Seems that something is not OK with your installation Bye Murof |
|
If this Information really helps, you could use the Rate function |
|
| 11/26/2025 4:04 AM | |
|
Joined: 9/23/2025 Last visit: 12/23/2025 Posts: 3 Rating:
|
@ToniVK |
| 11/26/2025 11:16 AM | |
|
Joined: 8/14/2020 Last visit: 12/18/2025 Posts: 379 Rating:
|
Hello
Which Unified version are you using exactly? When you start the simulation, have you checked if the project is running in the Runtime Manager afterwards, i.e., if the green circle is visible? https://docs.tia.siemens.cloud/r/en-us/v21/simatic-runtime-manager-rt-unified/the-runtime-manager-user-interface-rt-unified This is one of the basic requirements for logging in via the browser. Best regards, Costanza |
Follow us on