(0)| 4/30/2025 5:55 AM | |
|
Joined: 1/1/2017 Last visit: 10/30/2025 Posts: 343 Rating:
|
Dear Team, We have several Sirius Softstarters with MLFB 3RW5243-6TC14. When we are trying to configure the GSDML file v2.0 with ABB DCS 800XA, error message is coming that: “IO devices do not support the CI871 redundancy (HW tree pos: 26,27,…..) Row 1, Column 0” CI871 is the Profinet communication module from ABB DCS end which supports S2 type redundancy to get the Softstarter device nodes communicate with the DCS side. But the available GSDML have only S1 compatibility. Please let me know where I can get the S2 type GSDML file of the 3RW5243 softstarter. Regards OmKris https://support.industry.siemens.com/cs/ww/en/view/109757790 AttachmentGSDML-V2.35-Siemens-3RW5-20201216.zip (343 Downloads) |
Last edited by: OMKRIS2017 at: 04/30/2025 05:55:53Last edited by: OMKRIS2017 at: 04/30/2025 05:58:38Last edited by: Moderator_Lan at: 04/30/2025 07:32:04link optimized Last edited by: OMKRIS2017 at: 05/03/2025 14:02:00Redundancy Type Required |
|
Follow us on