6/29/2006 3:41 PM | |
Posts: 5822 Rating: (412)
|
Hello Mark, well to tell you the truth it was a guess, the thing with the PM. I have a ET 200 S COMPACT 16 DI / 16 DO in front of me and there I know I had to connect all Power Inputs, as it is shown on the COMPACT Module itself. It might have been that the PM of the Head module is not connected through to the Bus interface and in this case you would have to usea PM. http://support.automation.siemens.com/WW/view/en/22167495 Best regards J_Bell |
6/30/2006 8:56 AM | |
Posts: 8 Rating: (0) |
Thanks for your help. Mark |
Follow us on