(0)| 10/1/2012 5:26 PM | |
|
Joined: 6/4/2008 Last visit: 11/25/2025 Posts: 1521 Rating:
|
Hi, a quick point, the drive should show 009 before it will switch on. 009 means Ready for switch on. The reason you are seeing a 008 can be one of a few things: You may have an internal hardware fault (usually associated with an intermittent A017 alarm), but more likely, you will need to checkthe input binnector values of the parametersP555 to P564. The best way of viewing this status in one is to look at r550 and see that it matches the attached extract. If one of the bits are missing i.e. bit 3, then you know to look at P561 and trace back from there. Hope that helps. Regards, Graeme
AttachmentPages from vc34 Basic Function Diagrams.pdf (1204 Downloads) |
| 11/2/2025 8:54 AM | |
|
Joined: 11/2/2025 Last visit: 12/10/2025 Posts: 4 Rating:
|
perfect and everything is ok regarding your information |
Follow us on